This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO3088: Reliabilty FIT data for this device

Part Number: ISO3088

Hello,

My company is doing a product MTBF for a product launch of our solar inverter, and I was looking for the FITs rate for the ISO3088, ISO1050, ISO1540.

I went to the reliability database which has most parts, but these devices do not have any data.

Vince Bartlett

Consulting for Alpha Technolgies

  • Hi Vince,

    We will check this data internally and get back to you at the earliest.
    Thank you.

    Regards,
    Anand Reghunathan
  • Hi Vince,

    Please find the data below. Let me know if anything else is required.
    ISO3088: 0.8
    ISO1050: 0.6
    ISO1540: 0.4

    Regards,
    Anand Reghunathan
  • In reply to Anand Reghunathan:

    Dear Mr. Anand Reghunathan,

    Thank you can you add this following data so we can adjust the FIT data to our system which might or might not be at a higher temperature.

    Also the confidence rate will help since we use 90% rate which we can convert from a lower confidence rate

    ISO3088: 0.8   operating temp C =,  Confidence level = 60%, 90%?
    ISO1050: 0.6   operating temp C =,  Confidence level = 60%, 90%?
    ISO1540: 0.4   operating temp C =,  Confidence level = 60%, 90%?

    Vince Bartlett

    Consulting for Alpha Technolgies

  • In reply to Vincent Bartlett:

    Hi Vince,

    For all three parts
    Operating Tempearture = 55C
    Activation Energy = 0.7eV
    Confidence Interval = 60%

    Hope this helps.

    Regards,
    Anand Reghunathan
  • In reply to Anand Reghunathan:

    Thanks that's what we needed

    Vince Bartlett

    Consulting for Alpha Technolgies

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.