hi
i have used the ISO7321 in the FAN control and monitor,and the ISO7321-q1 use to isolate from high voltage domain and low voltage domain,the low voltage domain is 3V3,the GND is digital ground,and the high voltage is 5V,and the GND is -48V(the FAN array power supply is 0V),for the detail,please see the figure 1.
figure 1
but up to now there are at least 5 chips was damaged,the high voltage domian(the pin5,6,7,8 get together short,and the pin7 was black),but sometimes,the pin7 get together short whit pin8,
by the way,if this case was happen,the fuse on the power supply always damage.
please help me to solve the problem,thanks