• Resolved

ISO7763: Low-Frequency PWM signal

Part Number: ISO7763

Dear All,

our customer would like to use the ISO7763 for isolating a PWM motor control signal.

It is expected to have a signal of some kHz with high and low duty cycle. Will the ISO7763 have any problems with that?

I do not think so, as the d/s states that it could be used from '0Mbps' on.

But kindly asking to confirm.

Thanks and best regards

Does this post answer Your question? Please mark it with the "Verify Answer" button.