• Resolved

ISO7341FC: Input threshold for ISO7341

Part Number: ISO7341FC

Hi support team,

I have a question regarding ISO7341 input thresholds. The Electrical characteristic table has specified:

However, the timing diagram in Figure 14 showed the input threshold is VCC/2 ± VI(HYS), may I know which one is correct?

Thank you.

Best Regards,

Wei-Hao

  • Hi Wei-Hao,

    The table in section 7.9 of datasheet lists VOH & VOL which are the voltage levels that ISO7341 OUTx channels output. The recommended input voltage levels VIH & VIL that should be applied to input channels of ISO7341 is given in section 7.3 of datasheet as shown below.

    The timing diagram in Figure 14 is related to switching characteristics measurement where propagation delay is measurement from 50% point of input signal to 50% point of output signal. The 50% point is used for propagation delay measurement and not be mistaken for input thresholds. Thank you.

    Regards,

    Koteshwar Rao

  • In reply to Koteshwar Rao:

    Hi Koteshwar,

    My apologies for copying the wrong table and thank you for your clear explanation. It solved my concerns.

    Thank you

    Best Regards,

    Wei-Hao