This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7741: Supply Current for Entire Device or Per Channel?

Part Number: ISO7741

Do the ICC1 and ICC2 values in the datasheet represent per-channel values or total current for the device? For example, if VCC1 is 5V, all inputs are high, is ICC1 = 1.5mA, or 3x1.5mA = 4.5mA?

Thank you.

  • Hi Dustin,

    Thank you for posting your question on TI E2E forums!

    The Icc1 and Icc2 values in the datasheet represent the total current ( accounts for all channels) for the device under the test conditions specified.

    Hope this helps. Please  let us know if you have any other questions.

    Thank you,

    Abhi

  • In reply to Abhi Aarey:

    Abhi, thanks this is helpful.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.