This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISOW7821: PIN definition

Part Number: ISOW7821

 pin configuration on page3 of ISOW7821 spec, PIN3 & 4 and PIN13 & 14 in the PIN function figure are different from the diagram, which is the correct?

  • Hi Zhang,

    Thank you for pointing us to the discrepency in datasheet description. The pin diagram represents the correct pin-out of the device and the pin function table has wrong pin numbers assigned. This was the case for the datasheet revision released in Nov 2017, it is now fixed in the revision released in Mar 2018. Please download the latest datasheet for device ISOW7821 and you should see this mismatch fixed.

    Thanks again for letting us know about this.


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.