This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7342C: ISO7342CQDWRQ1 - Reliability Data

Part Number: ISO7342C

The http://www.ti.com/quality/docs/estimator.tsp does currently not provide any data about the Digital Isolators. I notice that behavior already in the past and sometime later (few month) the data were available again. Is there a data base available where I can check the values independent of the MTBF estimator?

Currently the device of  interest is: ISO7342CQDWRQ1

  • Hi David,

    Unfortunately we are still having issues with our online reliability tool (the irony is not lost on me). For the time being please bring your reliability questions to E2E and we will be happy to manually look up the information for you.

    Part number MTBF FIT Usage temp (°C) Conf level (%) Activation energy (eV) Test temp (°C)
    ISO7342CQDWRQ1 2.48E+09 0.4 55 60 0.7 125

    Please let me know if you have any questions. 

    Best regards, 

    Dan

  • In reply to Dan Kisling:

    Because I have to calculate the FIT Rate for 30°C and 90% confidence, I need additional Information about how the 0.4 FIT has been tested.

    * Test duration

    * Sample Size

    * Number of Fails

    This are the MTBF/FIT supporting data usually provided by the MTBF estimator.

    (could you provide the same table as in: e2e.ti.com/.../684390 ?)
  • In reply to David Beyeler:

    Hi David,

    I should have recognized your username! I'll try to remember next time you ask to give you all of the numbers up front.

    Part number MTBF FIT Usage temp (°C) Conf level (%) Activation energy (eV) Test temp (°C) Test duration (hours) Sample size Fails
    ISO7342CQDWRQ1 2.48E+09 0.4 55 60 0.7 125 1000 57882 0

    Best regards, 

    Dan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.