This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ISO7721: about total current consumption

Intellectual 1420 points

Replies: 1

Views: 336

Part Number: ISO7721

Hi team

the below current is for each VCCx.

it is Max 1.6mA.

so I has to double it for total current consumption including VCC1 and VCC2 

and total current consumption will be 3.2mA(= 1.6mA x 2 ) ?

  • Hi Paul,

    Your understanding is correct. ICC1 & ICC2 each will be max 1.6mA and the total current would be the sum of both which in this case is [double of 1.6mA] = 3.2mA. Thanks.


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.