This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO1212: To replace the opto coupler

Expert 4710 points

Replies: 2

Views: 601

Part Number: ISO1212

ISO guys,

Is it possible to use ISO1212 replacing the opto-coupler on the motor driver application as below shown?

The diagram shows the commonity interface between PLC and Servo motor driver.

It means that the ISO1212 needs to meet AM26C31 line driver's output characteristic!!

Also, Is there any similar application or successful story in the WW?

AC Inverter

Brian

  • Remove

  • In reply to Brian Wang0928:

    Brian,

    The ISO1212 can be used to replace the optocoupler for a similar application but the differential signal on the input side needs to be greater than 10V.  The AM26C31 does not appear to be able to provide this level of differential signal. There is a Tech Note here that covers the application of the ISO121x in motor drives. 

    Respectfully,

    Lucas Schulte

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.