This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7741-Q1: Where are the package dimensions located?

Prodigy 60 points

Replies: 1

Views: 448

Part Number: ISO7741-Q1

I cannot find them in the datasheet, the PDF package files only contain a 3D drawing and there is no .bxl file available.

  • Hi Francis,

    I am sorry that you couldn't find package related information of ISO7741-Q1 from its datasheet. The datasheet usually includes detailed package information, for ISO7741-Q1 it seems like this data went missing just recently. Thank you for reporting this to us, I will with the respective team to get this fixed as soon as possible.

    Meanwhile, please refer to ISO7741 non-Q1 datasheet which includes all the package information and the information is going to be similar to ISO7741-Q1. After looking at ISO7741 datasheet, if you still have any questions please feel free to reach out to us. Thank you.


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.