This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ISO5500EVM: Not getting the input pwm signal at output side.

Prodigy 55 points

Replies: 8

Views: 870

Part Number: ISO5500EVM

I am trying to drive a n-mosfet (30n60 IC) with ISO5500EVM. The issue is, I am not getting the control signal given to input put PIN (TP4) in the left side at output side .(Vout in the right side)

My connections are

left side
5 Volt between TP10 and TP9
control signal to TP4
TP3 and TP4 are connected to the ground

right side
S, D, and G points are connected to source , drain and gate of the mosfet. And a load is connected to the mosfet and 20 volts is given between the mosfet and the load.
15 Volt is given between TP12 and TP11

It would be really helpful if you could let me know the correct connections.

 

  • Hi Siddiq,

    My colleague who supports this part is out of the office. Let me find out when he is back to help you with this.

    Best regards,

    Don Dapkus

    Gate Driver Applications Engineering Manager

    Dallas, TX USA

  • Hi Siddiq,

    It may due to incorrect connection on the DESAT pin. Could you please try to connect JMP2 to see if you can get an output?

    Also could you draw a schematic of the MOSFET connection to the external 20V supply? 

    With Regards,

    Xiong

  • In reply to Don Dapkus:

    thanks

  • In reply to Xiong Li:

    This is my conenction . I have connected JMP2 and still not getting the output signal at Gate . 

  • In reply to Siddiq Akbar:

    Hi Siddiq,

    There is a UVLO function on the VCC2 side which may have disabled the driver output. Can you measure the voltage between VCC2 and VE?

    Also, can you try?

    1. Please connect VIN- to GND1.
    2. Please connect JMP8.

    Let me know how it goes.

    With Regards,
    Xiong
  • In reply to Xiong Li:

    Hi xiong,
    I have tried connecting VIN- to GND1 and JMP8. Still i am not getting the input signal at gate pin.
    voltage between VCC2 and VE is 0V.
  • In reply to Xiong Li:

    am i supposed to get the input signal between gate pin (G) and drain pin (D) of iso5500evm if i dont connect the Mosfet/igbt. I mean when nothing is connected to S, G, D pins .
  • In reply to Siddiq Akbar:

    Hi Siddiq,

    I am closing this thread as we are having discussions offline.

    With Regards,
    Xiong

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.