This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] Is there reliability fit data available for the ISO1211 and the ISO1212 digital input receiver devices?

Prodigy 380 points

Replies: 1

Views: 803

Is there reliability fit data available for the ISO1211 and the ISO1212 digital input receiver devices?

  • FIT data is a measurement of reliability and depends on the process through which the integrated circuit is made. Please refer to this thread and the table below for the the FIT for the ISO121x family of isolated digital input receivers.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.