This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7740: ISO7740

Prodigy 20 points

Replies: 2

Views: 250

Part Number: ISO7740

Hello,

 I use ISO7740. VCC1=5V,  VCC2=3,3V.

Are such operating modes acceptable?

  • ISO7740. VCC1=5V, VCC2=3,3V.

    Are such operating modes acceptable?
  • Hi Vitaly,

    Thank you for your interest in ISO7740.
    Yes, the power supply configuration you have mentioned is acceptable. You can find more information regarding this topic at the link below.

    e2e.ti.com/.../732656


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.