This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO721M-EP: IEC 60747-5-2 characteristics 10M-ohm Isolation Requirement

Part Number: ISO721M-EP

Hello, 

On the bottom of page four of the data sheet, it lists an IEC 60747-5-2 characteristics (Rs) which doesn’t explicitly meet the 10Meg isolation requirement.  On page 12, it lists the package characteristics (Rio) which does meet the 10Meg isolation requirement.  Can you confirm which value is correct and if it is the value on page 12, can you explain why the value on page four is less?  

Thanks,

HSG

  • Mark, I am not very familiar with the IEC specification.
    However, you indicate it does not meet a 10Mohm requirement? The page four spec indicates greater than 10^9 ohms. This is greater than 1 Gohm.
    On the surface, I do not see the discrepancy. Let me know if I am misunderstanding something.

    Regards,
    Wade
  • In reply to Wade Vonbergen:

    Hi Wade,

    You are totally correct. It is a busy day.

    Thank you,
    HSG

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.