This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7740: Wide-body SOIC package

Prodigy 160 points

Replies: 2

Views: 140

Part Number: ISO7740

Hi,

I have a question.(Customer inquiries)

Is there a 16 - pin package with increased creepage distance in the ISO77xx series?(side A ≧12.5 mm)

Do you have any plans?

Best regards,
Morita

  • Hi Morita,

    Currently ISO7740 is available with max creepage/clearance of ~8mm in WB SOIC-16 package (DW is the package code). Alternatively, we have ISO7840 in ultra wide body SOIC-16 package that has creepage/clearance of ~14mm . Please recommend customer to use ISO7840DWW (DWW is the package code), thanks.


    Regards,
    Koteshwar Rao

  • In reply to Koteshwar Rao:

    Hello Koteshwar,

    Thanks for your quick reply.

    I understand.

    Best regards,
    Morita

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.