ISO7421: ISO7421 failure on one transmission

Part Number: ISO7421

Hi,

I just got a claim from a customer regarding communication problems which is caused by a defect of an ISO7421.

The electronic environment is between -20°C and 25°C (it's truck trailer with built in refrigerator) and is sealed with a protection paint. Ground shifts are at a maximum of 70V.

Is there any known issue with this kind of isolators? Is it possible to send the device in to TI for further analysis?

kind regards

Tobias

10 Replies