This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ESD/EFT Protection Component Selection

Prodigy 70 points

Replies: 1

Views: 89

Hi,

We are designing a custom board with following interfaces 

1) SD Card

2) UART

3) USB 3.0

4) 1G Ethernet

Also, we have NC-SI interface running from one board to another via BTB connector.

We need to meet the following compliance:

1) IEC/EN 61000-4-2 (ESD)

2) IEC/EN 61000-4-4 (Transients)

3) IEC/EN 61000-4-5 (Surge)

Can we use TPD6E05U06 for both SD card and UART interface? 

Do we need to consider adding protection components for the signals running to different board via any BTB connector?

Can anyone guide to select or refer any Protection components to meet these compliance?

  • Hello,
    While you can use that device we have recommendations for other devices to fit those interfaces
    www.ti.com/.../sszb130c.pdf
    www.ti.com/.../sllt213a.pdf

    Regards,

    Cameron Phillips
    Applications | c-phillips@ti.com
    High Side Switches/ESD & Surge Protection

    If this answers your query, Please click "This resolved my issue" button.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.