• TI Thinks Resolved

ISO1540: Waveform Discussion

Expert 7095 points

Replies: 1

Views: 62

Part Number: ISO1540

Dear Team,

Is there any way we can fix the waveform here?

BR

Kevin

  • Hi Kevin, 

    This is expected behavior for the ISO1540 Logic LOW level output. VOL1 may be up to 0.8V on Side 1 on the ISO1540 bidirectional I2C isolator.

    More information about this can be found at the following FAQ:

    Best regards, 

    Dan