This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7641FC: To know whether the ISO7641FC has apply IEC62368-1 A3

Part Number: ISO7641FC

Hi Expert,

The customer who make the power supply is asking the certification : IEC62368-1 A3 of ISO7641FC.

Pls let us know the status.

Best regards,

Eric Lai

 

Field Application Engineer

Texas Instruments Taiwan Limited

O: +886-2-2175-2582

M: +886-909-262-582

E-Mail:Eric.Lai@ti.com   

  • Hi Eric,

    Thank you for using E2E.
    ISO7641FC is one of our older generation devices, i would recommend looking at ISO7741F for any new requirements to take advantage of all the performance improvements achieved in ISO77xx family.

    I see that IEC 62368-1 is a new safety standard for audio-visual (AV) and information & communication technology (ICT) components and equipment. I am not very familiar with the standard but I see this standard is based of and is going to replace IEC 60950-1 and IEC 60065. The device ISO77xx complies to both IEC 60950-1 and IEC 60065 as given in Section 6.7 of ISO7741 datasheet. I am not sure if this answers your question but if I do find more information on this topic, I will come back and update it here. Thanks.


    Regards,
    Koteshwar Rao
  • Hi Eric,

    ISO7641FC is certified according to IEC 60950-1 2nd Ed already. This is an active standard.

    There is currently no plan to certify this device according to IEC 62368-1 (which will eventually replace IEC 60950-1).

    Saleem Marwat

    Systems Engineer

    Isolation Products, Texas Instruments

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.