This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7762: FIT rate of Digital Isolators

Part Number: ISO7762

Dear Team,

is it possible to get FIT rates of our digital isolators (in this case the ISO7762)?

The online tool on http://www.ti.com/quality/docs/estimator.tsp does not bring results for this component.

The data sheet mentioned >40 years Isolation Barrier Life, but whats about the complete device?

Thanks and best regards

Martin

  • Hi Martin,

    I am sorry that the reliability tool currently doesn't support isolators, please find below the reliability data for ISO7762.

    MTBF : 2.50E+09
    FIT RATE : 0.4
    CONF LEVEL : 60%
    USAGE TEMP : 55C

    For the overall device lifetime qualification we follow the standard industry practice and qualification tests includes HTOL, HAST and others. These tests do not directly convert to a particular lifetime but it is considered satisfactory across the industry. I hope this answers your questions, thanks.


    Regards,
    Koteshwar Rao
  • Koteshwar,
    thanks a lot for the fast answer!
    Best Regards
    Martin