This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO1212: Reliability data

Prodigy 230 points

Replies: 2

Views: 875

Part Number: ISO1212

Hi,

Is there reliability fit data available for the ISO1211 and the ISO1212?

Regards

  • Ronald,

    Here is the FIT for the ISO121x shown in the table below. Please let me know if have any more questions.

     

     

    MTBF / FIT

    MTBF / FIT supporting data

    Part number

    MTBF

    FIT

    Usage temp (°C)

    Conf level (%)

    Activation energy (eV)

    Test temp (°C)

    Test duration (hours)

    Sample size

    Fails

    ISO121x

    2.02E+09

    0.5

    55

    60

    0.7

    125

    1000

    47098

    0

    Respectfully,

    Lucas Schulte

  • In reply to Lucas Schulte9:

    Lucas,

    Thanks!

    Regards

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.