This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7220C:ISO7220C能将1.3V~5V转换成0V~3.3V吗?

Prodigy 20 points

Replies: 2

Views: 467

Part Number: ISO7220C

有个项目需要用串口通讯,输入端波形电压为5V~1.3V,请问有哪款产品可以将此电压转换为3.3V~0V ?

同理,反向也需要将0V~3.3V转换为0V~5V或者1.3V~5V都行;

期待您的解答!感谢!

  • Hi,

    I tried to translate your post to English and this is how it converts.

    "There is a project that needs to use serial communication. The waveform voltage at the input end is 5V~1.3V. Which product can convert this voltage to 3.3V~0V?
    Similarly, the reverse also needs to convert 0V~3.3V to 0V~5V or 1.3V~5V;
    Looking forward to your answer! thank!"

    I am assuming this translation describes your question accurately. TI has quite a few voltage level translators that can be used to level translate different voltage signals. For a suitable device recommendation, please post your query in English at the below link.

    e2e.ti.com/.../

    If you prefer to post it in your local langauge then you can use the below link to post your question.

    https://e2echina.ti.com/

    I am also translating my complete post to Chinese language in case if you are not able to interpret my response in English completely. Thank you.

    Regards,
    Koteshwar Rao


    嗨,

    我试图将你的帖子翻译成英文,这就是它的转换方式。

    “有一个项目需要使用串行通信。输入端的波形电压为5V~1.3V。哪个产品可以将此电压转换为3.3V~0V?
    同样,反向也需要将0V~3.3V转换为0V~5V或1.3V~5V;
    期待您的回答! 谢谢!”

    我假设这个翻译准确地描述了你的问题。 TI拥有相当多的电压电平转换器,可用于电平转换不同的电压信号。 如需合适的设备推荐,请在以下链接中以英文发布您的查询。

    e2e.ti.com/.../

    如果您希望将其发布在当地语言中,则可以使用以下链接发布您的问题。

    https://e2echina.ti.com/

    如果你不能完全用英语解释我的回答,我也会将我的完整帖子翻译成中文。 谢谢。

    问候,
    Koteshwar Rao
  • In reply to Koteshwar Rao:

    Thank you for your reply. I'll find a voltage level translators, Thank you again!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.