This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 6
Views: 837
Part Number: ISO7641FC
Hi,
I would like to know Life Expectancy vs Working Voltage of ISO7641 as below(ISO7420FD datahseet), however it is nothing on the datasheet.
Could you share it if you have the data?
Best Regards,
Kuramochi
In reply to Abhi Aarey:
In reply to TQ:
Hi Kuramochi-san,
No I didn't meant that - I suggested ISO77XX family and ISO78XX family because they have high lifetime and good working voltage capability.
For ISO7641FC, the only data we have is average lifetime
For an actual working voltage of 63V, the average lifetime expectancy for the ISO7641FC is ~285.38 years [ 9 * 1E9 seconds].
Hope this helps!
Thank you,
Abhi