This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ISO1050: How the galvanic isolation is actually created? Can you reveal anything about materials and structure?

Prodigy 10 points

Replies: 1

Views: 339

Part Number: ISO1050

Dear Sir or Madam,

Datasheet mentions that there is a capacitive galvanic isolation and distance trough the insulation is 0.014mm. Now, I was wondering, could you reveal bit more detailed information about the structure that creates the actual isolation? To be more specific:

- How many isolation boundaries there really are? Just one or several? If there are several boundaries are they identical?  

- What is the material that creates the actual insulation? Kapton tape as in optocouplers OR glass OR vacuum OR something else?

- Do you have any kind of picture of the structure, you could share?

I am asking this because national certification agency states that ISO1050DW do not meet over voltage category III (OVCIII) in system voltage 300V if IEC 62477-1 considered...

(IEC 62477-1 is the successor of IEC 60950-1) 

  • Jouko,

    See the first section of this presentation for a clear understanding of our isolation architecture. In short, our digital isolators achieve isolation through 1 or 2 capacitor stages with a SiO2 dielectric for basic or reinforced isolation respectively. Also, have you seen the ISO1042? It is our newest CAN transceiver and can provide reinforced isolation.

    Respectfully,

    Lucas  

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.