I would like to generate a 10V isolated supply with the 6501, the input could be 5 or 3.3V. The output current is 8mA max with transients in the 0.5mA range.
Is there a recommended transformer for this application? I see the voltage doubling circuits in the datasheet but no recommendation for a transformer for this type of circuit (unless I missed it)
Thank you