Is there SN6501 efficiency graph for 350mA_max condition?
Datasheet is only 100mA_max condition.
Input and Output condition is 5Vin ⇒ 4~4.5Vout/ 200mA.
I want to find reference efficiency data for high current.
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there SN6501 efficiency graph for 350mA_max condition?
Datasheet is only 100mA_max condition.
Input and Output condition is 5Vin ⇒ 4~4.5Vout/ 200mA.
I want to find reference efficiency data for high current.
Best regards,
Satoshi
Satoshi-san,
Below is efficiency data for the SN6501 measured using Vcc = 5V and N = 1.1 transformer turns ratio, with no LDO. This system is identical to setup 2 in the SN6501 Multi-transformer EVM, which can be ordered for testing possible combinations of an SN6501 system.
The output voltage will vary based on load current when an LDO isn't used - like in this case - and different transformers will also affect the shape and value of this curve.
For your reference, the test data is provided in a spreedsheet attachment below.
I hope this is helpful! Please let me know which additional data will help for your design.
Thank you for choosing TI,
Manuel Chavez