Other Parts Discussed in Thread: EV2400
Hi,
We are trying to isolate the EV2300 SMBus by using the ISO1540. The circuit implemented is identical to the one in the ISO1540 datasheet (page 24). One side of the IC is being powered via the EV2300 board itself, whilst the other with an external 3.3 V supply. The problem is that no output is being observed on the ISO1540 when the EV2300 is transmitting. These is what we have done so far:
1) Tested the circuit with a function generator at the clock frequency of the EV2300. This worked perfectly.
2) Inserted a buffer between the EV2300 and the ISO1540. This also worked perfectly, but at the cost of bi-directional communication (which is useless).
The problem seems to arise when the EV2300 is connected directly to the ISO1540 (with the circuit explained above). Can you point me to the source of this problem and perhaps suggest a solution?
Thank you and regards,
Daniel