Hi,
We are designing a custom board with following interfaces
1) SD Card
2) UART
3) USB 3.0
4) 1G Ethernet
Also, we have NC-SI interface running from one board to another via BTB connector.
We need to meet the following compliance:
1) IEC/EN 61000-4-2 (ESD)
2) IEC/EN 61000-4-4 (Transients)
3) IEC/EN 61000-4-5 (Surge)
Can we use TPD6E05U06 for both SD card and UART interface?
Do we need to consider adding protection components for the signals running to different board via any BTB connector?
Can anyone guide to select or refer any Protection components to meet these compliance?