Other Parts Discussed in Thread: SN6501
The data sheet for the SN6501 list the supply current @ ~300uA. In the configuration below I would then expect to see about 1.5mA consumption (10k load (1.2mA) plus supply current). But I am measuring about 7mA. I am assuming the load from the windings in the 7603900014 and the diodes are causing the additional current draw.
The efficiency rating show about 85% based in voltage output and load current, therefore I would an additional 1mA @85% not 6mA.
Is there any way to get this circuit to function closer to a 2mA total draw?