Dear TI Support,
I am reviewing a design: The design has a signal flow that has a 48MHz data line going through a ISO7763 and then to a SN74AXC8T245RJWR . The isolator is powered at 3.3V on both sides, and the level translation goes from 3.3V to 1.8V The signal is UART data at 48Mbps (20.833ns). I was curious as to what speed a ISO7763FDBQR can go from INE to OUTE? Is the propagation delay symmetric? The PWD Pulse Width Distortion can be as much as 5ns at 3.3V. Is there a version of this isolator that can be powered on one side at 3.3V and 1.8V on the other side and that will work for a 48Mbps signal? It would eliminate the level shiftier.
Thank you very much for your help and support,
Jeffrey Cohen