I added a high voltage protector (http://ww1.microchip.com/downloads/en/AppNotes/AN-D66.pdf to the input of ISO1211, hoping to limit the input current to less than 10mA to prevent accidental high voltage applied to the inputs, but it doesn't work as I expected
When bypassing the protection circuit, ISO1211 works fine when I apply 30V to it (it outputs 1), but with the protection circuit, ISO1211 outputs 0 when I apply 30V to the input.
Anything I missed here?
Note: Please ignore the inaccurate symbol for the N-Channel Depletion-mode MOSFET
Thanks for any pointer!