This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO3082: ISO3082 application problems

Intellectual 840 points

Replies: 1

Views: 158

Part Number: ISO3082

Hello:

ISO3082 has encountered some problems in use. I need your help.

1. Prepare to connect DE and RE# pin directly to AST2500 GPIO pin for control, I wonder if it is ok?

2. When R,D pin is connected to AST2500 RXD and TXD pin, do I need to exchange pin?

3. Can both VCC1 and VCC2 use 3.3v power?

ISO3082_Schematic.pdf

Best Regards

Leon

文晔集团

广东省深圳市南山区高新中三道9号环球数码大厦12

Mobile:(86)159 8985 2994

Tel:(86)755-26743880  Ext:6643

Fax:(86)755-26743990

  • Hi Leon,

    Please find below my inputs.

    1. Yes, DE and RE\ can be connected together to one GPIO pin of MCU for direction control without any issues. This is also described in Figure 27 under Section 9.2 of ISO3082 datasheet.

    2. Yes, R should be connected to RXD pin while D should be connected to TXD pin of the MCU.

    3. Unfortunately, ISO3082 VCC2 can only be operated with 5V±10% supply and it doesn't support 3.3V. Instead I would recommend using ISO1410 which is our latest isolated RS-485 transceiver that supports both 3.3V & 5V operation on the bus side (VCC2) while VCC1 can be operated for voltages 1.8V, 2.5V, 3.3V or 5V irrespective of VCC2.

    ISO1410, being our latest isolated RS-485 transceiver, has many advantages over ISO3082. Please refer to the below E2E post to know more about the advantages of ISO1410 over ISO3082. Thanks.

    e2e.ti.com/.../787278


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.