Other Parts Discussed in Thread: ISO1042, , ISO1042-Q1
Hi Sir,
We now use ISO1050DUBR, there's a risk of short circuit between CANL and 24Vdc(system power supply).
Base on this, I made a test like that: When system on communicated, I shorted 24Vdc power to CANL pin, keeps 5 seconds, then disconnected keeps 5 seconds; repeat shorted and disconnected; after 5-6 times like that, communication interrupted. IC CANL impedance GND2 is about 100 ohms.
then, this is my doubt: ISO1050DUBR bus fault voltage is -27~40V; how can I understand this value? why I add 24Vdc on CANL will damage the IC.
thanks for your attention, and wait for you.
regards.