Hi,
Currently we are facing an issue when using 2 isolator parts in parallel and trying to control 2 ADS129* parts in Daisy Chain Mode.
We are finding some issues as follows:
1, When we power up the board, we supply 3v3 to VCC1 of the ISOW part, and can read 3v3 on VCC2. As soon as we try write data to the ISO and ISOW parts, the voltage on VCC2 drops to 2V and never recovers, until we powercycle the board
2, When we try and write commands across either ISO part (ISO and ISOW) we do not read any data on the output of the isolator devices. We only get data across when we remove the parts and manually bridge the gaps with wire
3, I don't know if this is relevant to the Isolation forum, but our ADS129* are not working, as we do not get any activity on the DRDY pin when we remove the isolators.
Many thanks,
James