Hi,
I am trying to understand the circuit response with surge for ISO1212 , I used IEC61000-4-5_2K simulation file as surge input.Normal input to the circuit is 24V. I also used reference simulation file from TI for ISO1212 simlation.
Rin -562
Rthr- 2.8k
TVS used is SMAJ22CA
Here the curcuit is taking 500us of time to recover and come to normal operation.
in ouraplication, Filter time delay shall be less than 100uS. It would be gratefull if I get some help in this regard.
or If am doing some error in simulation
Attached the WIP simlation file. Kindly hep me.
Thanks and regards!!