• Resolved

ISO7710: About datasheet

Genius 5080 points

Replies: 2

Views: 72

Part Number: ISO7710

Hello support team,

I have a question about the datasheet of ISO7710.
Our customer pointed out it.

In Figure 18 on page 19, "INPUT" and "VCC" are shorted.
I think "INPUT" should be connected to pin 2.
I think it is a typo, how is it?
I think that the same part is wrong in the datasheet of ISO7710-Q1 too.

Sincerely,
M. Tachibana

  • Hi Tachibana-san,

    Thank you for reaching out to us and pointing out the typo in the datasheet. Yes, INPUT should be connected to Pin 2 (IN) of the device instead it is accidentally shorted to VCC line. I will get this corrected for both ISO7710 & ISO7710-Q1. Thanks.

    Regards,
    Koteshwar Rao

  • In reply to Koteshwar Rao:

    Hi Rao-san,

    Thank you for your prompt response.
    I expect these datasheets to be revised soon. 

    Respectfully yours,
    M. Tachibana