• TI Thinks Resolved

ISOW7841: automotive application use ISOW7841

Prodigy 50 points

Replies: 3

Views: 101

Part Number: ISOW7841

We are under analysis to use ISOW7841 in automotive and industrial application for isolated RS485 application, I have following questions, If you not the right person request you connect the right person 1. Weather this chip will meet AEC-Q200 (automotive qualifications)?. If not is any plan for AEC-Q200 qualification?. 2. Also need vibration limits and robustness information for this chip? 3. Recommend, similar Chip which is AEC-Q200 qualified Our product requirement

1. Operating temperature -40°C to 115°C

2.Vibration requirement - 17g

  • Hi Srinivasan, 

    Unfortunately, we do not comment on our road map devices on our public forum. Can I contact you with the email you used to sign up for E2E? I would be happy to discuss this further with you over a private communication channel. 

    Best regards, 

    Dan

  • In reply to Dan Kisling:

    Hello Mr Dan Kisling,

    Thank you for your reply,

    Could you please contact to my mail ID,

    Hope You can able to visible my email ID from my profile.

    Best regards,

    Elumalai Srinivasan

  • In reply to Srinivasan Elumalai:

    Hi Elumalai, 

    I have sent you an email offline. We will continue our discussion there. Thank you for asking your question on E2E!

    Best regards, 

    Dan