This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3082: How select capacitor value for signal GND PE isolation

Part Number: ISO3082

Hi All,

 What purposes for C12 and C20, how calculate/select its values? 

  • Xiaobing,

    Section 2.3 Transient Protection of the user guide explains the purpose of the these capacitors.

    The voltage rating of the capacitors must be able to handle the voltage of the surge event (2kV). The capacitance is chosen with a high enough value in order to transfer an effective amount of energy  between GND and PE. 4.7nF is a common value for this.

    Respectfully,

    Lucas