Greetings,
I am using ISO15DW 3.3V RS-485 Transceiver. Here is the schematic of my hardware:-
I have used dsPIC microcontroller for this purpose. When I directly connect RS485-RX and RS485-TX pins of dsPIC microcontroller(removing ISO15DW and R3,R6,C15 and C16) to USB-TO-TTL module then I am able to see dsPIC transmitted signals on UART terminal of my PC. However, when I place the ISO15 ic and other related components and connect to USB-TO-RS485 module then I am seeing only 0x00 on my UART terminal. Kindly tell me how to troubleshoot this issue.
Thanks
Best Regards
Bhushan