This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

PGA450-Q1: PGA450 datasheet interpretation

Prodigy 40 points

Replies: 2

Views: 3234

Part Number: PGA450-Q1

Support Path: /Product/Development and troubleshooting/

I'm having an issue with the PGA450 involving SPI communication.

My test setup:

SPI master: STM32F2

SPI phase: 2 edge

SPI polarity: 0

SPI wordsize: 8bit

The PGA450 eval board is connected the STM3 through a level shifter, to go from 3V3 TTL to 5V logic for the PGA450.

I'm trying to program registers within the ESFR. The first thing I do after PGA450 powerup is send a 0x16 0x2F 0x01 to put the onboard mcu into reset to allow for ESFR access. After another transfer, I get the following response to this command: 0x02 0x00 0x00. this would indicate that the command was successful.


Next, I try to read the current value of ESFR address 0xc0, as per the datasheet example. I send: 0x19 0xc0 0x00. Again, after another transfer, the response to this command is 0xc2 0x00 0x00. This would indicate a parity error.

What's going on here? As per datasheet example (Table 17) this is a valid command. Any ideas?

Chris

  • Chris,
    I am moving this to automotive forum where PGA450 is supported.
    Thanks,
    Vishy
  • Hi Chris,
    Since we had a call to discuss this issue in detail, I am closing the thread, and we will proceed with direct email support.
    For other viewers, the issue is likely due to a defective PGA450Q1EVM and/or TI-GER board.
    Akeem Whitehead // Texas Instruments // ASC-SENSING-SSC // Applications Engineer
    Visit our Ultrasonic Sensing FAQ page for additional information.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.