This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS2115A-Q1 1-sigma of "Hysteresis of IN2-IN1 comparator"

Hi

I want the +/-1 sigma value and median value for "Hysteresis of IN2-IN1 comparator" of TPS2115A-Q1.

Could you share me them?

If needed, I want to communicate directly.

BestRegards

  • Hi,

    I have checked the characterization and the mean value is 0.15 V and the single sigma is 0.00587.

    Best Regards,
    Scott

    Best Regards,

    Scott Monroe

    --------------------------------------------------

    For more information on Multi-Channel Power Management ICs: 

  • In reply to Scott Monroe:

    Hi Scott

    The information you offered was big help for us.

    You offered  +/-1 sigma value and median value for "Hysteresis of IN2-IN1 comparator" of TPS2115A-Q1.

    In addition, do you have information about these value at high-temperature.

    (At Ta=75C, if possible.)

    Or, it is OK for any value at high-temperature that you can share.

    Could you please consider it?

    BestRegards




    BestRegards

  • In reply to user4271222:

    Hello,

    Normally such detailed characterization results are part of a PPAP that is used by automotive customers and requested through our quality services once a device has been designed into an application and is considered proprietary information and not released on a public forum such as this. A local Field Applications engineer has reached out to me on this one so I will provide the high temp information to him who can pass it along to you.

    Best Regards,
    Scott

    Best Regards,

    Scott Monroe

    --------------------------------------------------

    For more information on Multi-Channel Power Management ICs: 

  • In reply to Scott Monroe:

    Hi Scott

    Thank you for your cooperation.

    BestRegards

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.