This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

How to run play store on TI-Android-ICS-4.0.3_AM37x_3.0.0 beagleboard-xM

Intellectual 425 points

Replies: 10

Views: 4699

Hardware : Beagleboard-xM rev.B

DevKit : TI-Android-ICS-4.0.3_AM37x_3.0.0

i use adb command install the play store 3.10.9 into targetboard and can see this application in list.

But when i run the play store , it not show any message and return ,

What process i need to do ?

  • Could you share the logcat output when you try to run the Play store app?

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to Vishveshwar Bhat:

    5074.playstore_log.txt

     

    attach file is logcat file , it seem can't start create account process ?

    For standard SDK, not include the account manager apk ?

    11-26 09:16:21.140: D/Finsky(1518): [1] 12.run: AuthenticatorException while adding account: android.accounts.AuthenticatorException: bind failure.

  • In reply to Lucas Lu1:

    I have solved this issue .

    SDK not include gapps package.

    We need get the gapps for ICS 4.0.3 package and push into targetboard.

  • In reply to Lucas Lu1:

    Hi,

    Could you explain where did you download the gapps for 4.0.3 and how you installed it?

    thanks for your help.

  • In reply to Sanahuja Guillaume:

    1. download the gapps for ics from here : http://goo.im/gapps

    2. uncompress the zip file

    3. move the system folder to the target board , example : asb push system /system

    4. change target board /system/etc/permission and /system/etc/app to mode 644

    5. reboot the target board

    6. make sure connect to internet (some time not connect , you can disable ethernet and re-enable ethernet , the status will be show connect)

    7. run play store , will into wizard mode to add account , enjoy it.

  • In reply to Lucas Lu1:

    thanks for your fast answer!

    In fact I am stucked with the network. I cannot connect through the ui, nor in command line (netcfg usb0 dhcp).

  • In reply to Sanahuja Guillaume:

    note that I am using beagle XM and TI devkit 3.0.0 prebuilt image.

  • In reply to Sanahuja Guillaume:

    Hi again.

    So I really have a problem with ethernet.

    When I install the demo image from TI, I can connect through usb0. On android I can configure my mail, see my mails and browse internet. The status says "ethernet connected".

    When I uncompress the gapps on the sd card and boot again the board, I still have a connection (ping google.fr works from the serial port). The status also says "ethernet connected". But the connection does not work in the browser or in email application. So I can not connect to play store...

    Any idea?

    Thanks for your help.

    Guillaume

  • In reply to Sanahuja Guillaume:

    >>The status also says "ethernet connected". But the connection does not work in the browser or in email application. So I can not connect to play store..

    Do you try in android setting menu , disable the ethernet and re enable the ehternet ?

    When you run the play-store , what message show you ?

  • In reply to Lucas Lu1:

    There are other finding by searching for "setprop net.dns1" in Android forum, but these 2 seems good ones,

    http://e2e.ti.com/support/embedded/android/f/509/p/119913/427001.aspx

    http://e2e.ti.com/support/embedded/android/f/509/t/200648.aspx

    Please click the Verify Answer button on this post if it answers your question
    _______________________________________________________
    Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.