This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Remote System Explorer problem

Expert 1345 points

Replies: 4

Views: 2530

Hi

I am working with CCS 5.2 with a TI ARM Cortex A8 target.  I am trying to connect to the target using Remote System Explorer (RSE) and have followed the instructions here:

http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Hands_on_with_the_SDK#Configuring_Remote_System_Explorer_.28RSE.29

I have got to the last step, where I am to “Right-Click the My Target EVM node and select Connect”. I should then see the target's RSA key fingerprint.  However, instead I see:

Failed to connect sshd on "<snip>": ProxyHTTP: java.io.IOException: proxy error: Service Unavailable

How can I fix this please?

BR

David

4 Replies

  • Hi

    I have progressed a little with this.  I have added the EVM to the proxy bypass list in CCS.  Now when I attempt to connect to the EVM using RSE I get:

    Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException: inputstream is closed

    How should I proceed?

    BR

    David

  • In reply to David Aldrich:

    The lab that is mentioned was developed with version 5.1 of  CCS. Here is a link to download that version of CCS.

    http://software-dl.ti.com/dsps/dsps_public_sw/am_bu/sdk/AM335xSDK/latest/index_FDS.html

    The 5.1 version has RSE support in it.

  • In reply to Schuyler Patton:

    Hi

    It turned out that the openssh packages were not included in my kernel image. I added those and RSE now connects to the target correctly.

    David

  • In reply to David Aldrich92784:

    Hi david,
    what do you mean openssh packages in your kernel images?
    mre

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.