This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS/TMS320f28377s: CCSv7 RTOS C2000 support

Intellectual 780 points

Replies: 10

Views: 9855

Part Number: TMS320f28377s

Tool/software: TI-RTOS

Hi,

i am having some issues with TI RTOS after updating to CCSv7.

first off all, when i open the .cfg file of my RTSC project i don't get the gui anymore, only the c++ script shows.

I got some compiler issues regarding the platform and target name

but i can't find what these setting should be. I tried to import some example projects from the tirtos_c2000_2_16_01_14_examples folder but no projects show up in my import dialog...

and last: i can't seem to download any software from ti because i get an 'ERR_RESPONSE_HEADERS_MULTIPLE_CONTENT_DISPOSITION' message from the website (

) but i suppose that will be fixed in a while...

Thanks 

Jan

  • This thread explains how to handle non-Concerto C2000 devices: e2e.ti.com/.../2164291
  • Jan Goris
    first off all, when i open the .cfg file of my RTSC project i don't get the gui anymore, only the c++ script shows.

    See CCS/TM4C129ENCPDT: .cfg File not recognized for how to get the XGCONF GUI to open a .cfg file.

  • In reply to Chester Gillon:

    Thanks Chester, this worked.

  • In reply to ToddMullanix:

    Hi Todd.
    So i installed sys/bios 6.50. (i suppose i don't have to install ti/rtos anymore when using this kernell ?). But i still can't build my project correct (can't locate package 'ti.uia.runtime') and i still can't import any examples to get my settings right.....
    When importing an example with CCS project import i get a 'Device is either null or is currently unrecognized by CCS' error...
  • In reply to Jan Goris:

    I did not realize you were using UIA (UIA is bundled in with TI-RTOS). You can get UIA stand-alone here: software-dl.ti.com/.../index.html

    After you install UIA, have CCS locate it and restart CCS, you can go into your project properties->General->RTSC and select UIA also.
  • In reply to ToddMullanix:

    thanks Todd, everything works fine now.
    I use the cpuload api in my code, i suppose this is why the uia package is needed ?

    Also, i still get the 'ti.target.C28_float does not match expected devkits.target.generic warning. Could you please veryfy this is ok and my settings for target and platform are ok because i still can't open any rtos examples...

    regards
    Jan
  • In reply to Jan Goris:

    What's the exact version of CCS you are using?
  • In reply to ToddMullanix:

    It's version 7.1.0.00016

    compiler version = 17.3.0.STS

    here is a picture of the rest of the setup with the warning on top:

    Regards,

    Jan

  • In reply to Jan Goris:

    Hi Jan,

    After a little playing, I replicated the warning. There are some cases in CC7.1 that I've seen that message and it was bogus...and this is one of them:( It is getting resolved in the next CCS version. If things are working fine, you can ignore it.
  • In reply to ToddMullanix:

    ok,
    thanks for the reassurance Todd.

    regards,
    Jan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.