This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4501-SP: power up over voltage

Prodigy 110 points

Replies: 4

Views: 1911

Part Number: TPS7A4501-SP

hi,

feedback resistors are calculated to 3.3V, but when power up the device there is overshoot to 3.6V and then dropping to 3.3V. the time from overshoot until stable is about 20uS

1. is this normal behaviour?

2. can i do anything to fix this?

the resistors I am using are 5.32K, 3.01K and compensation capacitor of 220pF.

I tried to increase the compensation capacitor to 820pF but no change.

please advise.

Thanks 

4 Replies

  • Hello Assaf,

    Is this with the EVM or your own design? Also what is load at startup?

    Thanks,
    Kyle
  • In reply to Kyle Rakos:

    sorry for late respond, i was on vacation.

    its not an evm.

    load is about 300mA

  • In reply to assaf matia:

    Hey Assaf,

    Are you able to measure the frequency response of the design?

    Overshoot can happen is the Phase margin is too low or the frequency response is too slow.
    Changing the compensation capacitor can help, but without a baseline its hard to know.

    One other thing I would ask you to try is increasing the load at start up so see if that helps.

    Thanks,
    Daniel
  • In reply to Daniel Hartung:

    Hey Assaf,

    Were you able to take measurements on the board?
    Did the issue resolve itself?

    Thanks,
    Daniel

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.