This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74LVC1T45-EP: leakage in power domains

Intellectual 1000 points

Replies: 2

Views: 1497

Part Number: SN74LVC1T45-EP

There is leakage in the VCCA and VCCB power domains for SN74LVC1T45.

if the 74LVC1T45-EP chip has improved this problem, or it still exists?

If there is a buffer with no leakage models in the two power domains

  • Emma,
    The EP and not EP versions of the SN74LVC1T45 are essentially the same. There are differences with temperature extension, and also the EP quality flow is different. EP has single baseline and enhanced product change notification.

    Are you referring to the static ICCA and ICCB parameters in the datasheet?

    For translation device with lower leakage. Are you needing catalog, or EP?
    Regards,
    Wade
  • In reply to Wade Vonbergen:

    Let me know if you need further information. Marking this post as closed.
    Regards,
    Wade

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.