Two different pins of the device require different resistance values to set the overcurrent limit (PCL) and the fold-back current limit (RCS). The CS pin resistor sets the fold-back current level and shorting CS low will disable the foldback current limit. I plan to short CS to ground to disable the foldback current limit, what do i need to do with the PCL resistor if i short CS to ground disabling the fold-back current level?