This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP 3530 USB1 problem

Prodigy 10 points

Replies: 1

Views: 2615

I need help to resolve the issue with OMAP 3530 USB1 OTG port problem.

I have connected USB1 ULPI port to external ULPI transceiver USB 3326. I am operating this port in Host mode with Linux version 2.6.31

What I see is - the USB port works as expected on about 50% of the boards built so far. However, on the remaining boards, I fail to see anything happening when I plug-in USB stick. I tried different USB sticks. Occasionally I get message saying "failed to enumerate device..." . I am not sure if it a hardware problem. The problem doesn't go away even if I swap the PHY or processor.

Any help will be appreciated.

Thanks,

1 Reply

  • Hi,

    Moving your post to right forum to be better answered.

    Thanks & regards,
    Sivaraj K
     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.