This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

understinaing nand ecc HW

Guru 20755 points

Replies: 1

Views: 3022

Hello,

I am trying to understand nandecc hw,

in

there is a table with column

1. hadrware error detection

2. driver solution - error correction

With omap35x for example it shows,

HW error detection support: 1(g),4 (pink?),8(g)

driver solution - 8,

My question:

1. Does driver solution here means hadware correction (not software) ?

2. How do we choose the hw error detection (between 1/4/8), or is it a feature of nand chip (and we can't change it) ?

3. if we have a chip with 4 ecc, does it means we use nand ecc 8 (driver). according to a comment in this page, this is not something good:

"

What will happen if an 8-bit ECC NAND is used with our 4-bit ECC capable devices?

In this scenario, if more than 4 errors are detected, the errors can't be corrected. This can have serious consequences including boot failure. It is advisable to keep correcting the ECC errors in the designated read-only/boot sections of the NAND to reduce the chances of boot failure.

"

4. I think the table shows that we use BCH8 only with omap35x.

So wht does there is errata with omap35x, which states "GPMC Has Incorrect ECC Computation for 4-Bit BCH Mode" ? Is it relavant ?

Regards,

Ran

==========

1 Reply

  • Hi Ran,

    I have moved your post to OMAP35x forum.

    -------------------------------

    Regards,

    Shankari

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.