This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Clock speed of OMAP5432 EVM (800/1500Mhz) ?

Prodigy 50 points

Replies: 3

Views: 2210

I notice in the final FAQ mention of limitation of clock to 800Mhz:

http://e2e.ti.com/support/omap/f/885/t/265212.aspx

Since /proc/cpuinfo doesn't show clock speed I am wondering if this limit is still in effect.

If the limit is in effect, any method to relieve it on the 5432 EVM board until reboot would be greatly appreciated. I am doing some benchmarking and would love to compare 1.5Ghz even if the board holds that speed until hard reset.

  • I've also dug through the source files in the SDK that might generate the used map5-panda.dtb file, but nothing seems to give away the frequency there.

    From serial console at early boot:

    U-Boot SPL 2013.01 (Jul 10 2013 - 00:00:05)
    OMAP5432 ES2.0

    ...

    U-Boot 2013.01 (Jul 10 2013 - 00:00:20)

    CPU  : OMAP5432 ES2.0
    Board: OMAP5430 EVM
    I2C:   ready
    DRAM:  2 GiB
    relocation Offset is: 7e101000
    MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
    *** Warning - bad CRC, using default environment

  • In reply to Ben Martin:

    The current Linux release is limited to 800Mhz. 

    1.5Ghz release is planned to be available by end of Sep 2013. Android release already supports 1.5Ghz operation.

    ----------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    ----------------------------------------------------------------------------------------------------------

     

  • In reply to Gaurav Agarwal:

    OK, Thanks! For anyone finding this in a later search, by board reports a BogoMIPS of around 1590 per core.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.